This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Albert,
The VBIAS can be used is cases where you have a floating sensor voltage. VBIAS is used to bias the sensor within the input range of the ADC. The most common type or sensor application that would use VBIAS is a thermocouple. Although other types of sensors can be used the VBIAS has limited sinking/sourcing capability.
Similarly the burn-out current sources (BOCS) are used for detecting opens/shorts in the sensor path and most commonly used with thermocouples.
I would suggest taking a look at A Basic Guide to Thermocouple Measurements:
http://www.ti.com/lit/an/sbaa274/sbaa274.pdf
Section 2.4 shows an example of VBIAS and BOCS with thermocouple measurements. There are other combinations also shown in the guide.
Best regards,
Bob B