This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Noushin,
The default MCLK frequency is 80MHz.
CLK frequency, DCLK frequency, and CLK_CFG frequency are derived from the respective count values referenced to MCLK (80MHz).
For example, the default count value programmed to CLK_HIGH and CLK_LOW is 7. Total count value is 2*(7+1) = 16. CLK frequency will be 80MHz / 16 = 5MHz.
Similarly, DCLK_HIGH and DCLK_LOW counts are 1. Total count value is 2*(1+1) = 4. DCLK frequency will be 80MHz / 4 = 20MHz.
In a similar way, you should be able to derive the CLK_CFG.
CONV is based out of # CLK counts. In the GUI, the default count value is 1600. That corresponds to 1600/5MHz = 320us.
To begin with, you can program the EVM GUI default values and read back the values and then adjust the values based on your application requirements.