Part Number: TSC2007
I am working with TCS2007 Touch driver ic which uses i2c protocol to communicate with my controller(Renesas s5d9) Based on touch IRQ was generated , i can able to read the TSC2007_MEASURE_TEMP0 and TSC2007_MEASURE_TEMP1 but i can't able to read the x,y position from the screen.
Any one can help me with this issue...
refer the command byte listed below
#define TSC2007_MEASURE_TEMP0 (0x0 << 4)
#define TSC2007_MEASURE_AUX (0x2 << 4)
#define TSC2007_MEASURE_TEMP1 (0x4 << 4)
#define TSC2007_ACTIVATE_XN (0x8 << 4)
#define TSC2007_ACTIVATE_YN (0x9 << 4)
#define TSC2007_ACTIVATE_YP_XN (0xa << 4)
#define TSC2007_SETUP (0xb << 4)
#define TSC2007_MEASURE_X (0xc << 4)
#define TSC2007_MEASURE_Y (0xd << 4)
#define TSC2007_MEASURE_Z1 (0xe << 4)
#define TSC2007_MEASURE_Z2 (0xf << 4)
#define TSC2007_POWER_OFF_IRQ_EN (0x0 << 2)
#define TSC2007_ADC_ON_IRQ_DIS0 (0x1 << 2)
#define TSC2007_ADC_OFF_IRQ_EN (0x2 << 2)
#define TSC2007_ADC_ON_IRQ_DIS1 (0x3 << 2)
#define TSC2007_12BIT (0x0 << 1)
#define TSC2007_8BIT (0x1 << 1)
#define MAX_12BIT ((1 << 12) - 1)
#define ADC_ON_12BIT (TSC2007_12BIT | TSC2007_ADC_ON_IRQ_DIS0)
#define READ_Y (ADC_ON_12BIT | TSC2007_MEASURE_Y)
#define READ_Z1 (ADC_ON_12BIT | TSC2007_MEASURE_Z1)
#define READ_Z2 (ADC_ON_12BIT | TSC2007_MEASURE_Z2)
#define READ_X (ADC_ON_12BIT | TSC2007_MEASURE_X)
#define PWRDOWN (TSC2007_12BIT | TSC2007_POWER_OFF_IRQ_EN)