This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW14J56EVM: A faster way to save data from capture card to PC

Part Number: TSW14J56EVM

Hello,

Currently, I am using TSW14J56EVM with ADS58J89 and Matlab automation codes to catch the data from the capture card and save it as .CSV format on my PC.

 The problem I have is saving data in .CSV format takes about couple of seconds. Is there any alternative way/automation codes to get to speed of ms?

Thanks for your help in advance.

  • Farshid,

    We are looking into this.

    Regards,

    Jim

  • Farshid,

    One workaround we recommend for this is to directly use the temporary bin files created by HSDC Pro. This file will be updated by HSDC Pro for every capture – this is where the captured date is saved for post processing & graphing by HSDC Pro. There will be one ‘.bin’ file per HSDC Pro channel. The file contains the channel data (samples in 16bit format) in this format: [Sample1 LSB] [Sample1 MSB] [Sample2 LSB] [Sample2 MSB]…etc

     

    The files can be found in this directory,

    C:\Users\Public\Documents\Texas Instruments\High Speed Data Converter Pro\HSDCPro Data

     

    Caution: The file reference needs to be closed (if opened in Matlab) before passing next capture even to HSDC Pro, otherwise HSDC Pro will crash as I won’t be able to open the file.

    Regards,

    Jim

  • Hello Jim,

    We have binary files from each channel as well as a .csv file containing all channels, and we are trying to match the decoded binary file to the csv file.

    If we consider the following order of bits in each sample:

    LSB: D0 D1 ... D7

    MSB: D8 D9 ... D15

    Then, D8 should be the sign bit.. However, this sometimes fails. For example, in the binary file, the 8 MSB bits of a particular sample is 11010111, which should translate to -41, but in the csv file it shows up as 215 (as if sign bit is completely ignored). 

    Does the sign bit change its position based on a certain rule, or are we decoding the binary file incorrectly? Also, I'm not clear on the meaning of the 8 LSB bits. Do they represent the decimal part of the number or something else entirely? The csv file only contains perfect integers. 

    Thanks

  • Farshid,

    I am looking into this.

    Regards,

    Jim