I am testing afe5832evm with TSW1400 and HSDC PRO 4.7.
However, I had some question during test.
-1. I connected the hardware as shown in the attached figure and input 5v power.
-2. I wrote afe5832evm firmware after running hdsc pro.
-3. The afe5832evm gui is run automatically,
4.I provide a 5MHz 20mV sine input
5 I use the 125MHz clock on board according to the user manual
6. I press DUT RESET and initialize device.
7. I changed fsamp to 40mhz and clicked the ramp test pattern.
8. I went back to hsdc pro and clicked the capture button.
Its results are as follows
What's wrong with my testing process? It was simply a test for confirming the test pattern.
How do i set up to get the right result?