Other Parts Discussed in Thread: HSMC-ADC-BRIDGE,
3326.HSMC-ADC-BRIDGE_RevB_sch.pdf
Hello,
I am trying to connect ADS4149EVM with Altera Cyclone-IV EVM board using HSMC-ADC-BRIDGE. But when I checked with schematics I see Pin numbers are not matching. For example As per the schematics D12_D13_P output of ADC board is connected to Pin 32 of J10 but in HSMC-ADC-BRIDGE INPUT12_P is connected to pin 96 of connector J2. So I do not understand how the connection gets established.
Please help on this issue.