Other Parts Discussed in Thread: DAC8775
Tool/software: Code Composer Studio
Hello. I am trying to set up a system using DAC8771. I made the electronic circuit according to EVM. I am sending data via SPI with STM32F407. However, the system does not work. The output voltage is always 0V.
AVDD / PVDD 12V.
VNEG + 140mV and VPOS + 3.3V on the BBC. VREF is set to 5V.
How to register. I tried to do it according to the datasheet but it does not happen. What should I do?