This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5263EVM: The maximum input frequency of J31 is 50MHz?

Part Number: ADS5263EVM
Other Parts Discussed in Thread: ADS5263

Hi,

When I read the datasheet of ADS5263, it captures the input signal at the both rising and falling edge of CLKP(CLKM). So, when I use a single-end input J31 of ADS5263EVM for feeding this clock, the maximum input frequency of J31 is 50MHz. Is this correct?

I wanted to use this ADC at 100MSPS, so I fed 100MHz of sine wave in J31 at first time. I'm afraid that this breaks the ADC or not, since I thought feeding 100MHz into J31 makes the ADC to sample at 200MSPS.

Best regards,

Yoshitaka