Hello.
On my board, I follow the instructions to get single tone output.
I adjust VCO frequency and VCO_LF voltage chenges to 3. I see that PLL is look.
But in output of DAC, negative voltage constant ~ -1V.
Then i set SPI constant SPIDAC to 0, and DACFS to 0, in the output i see frequency, with negative dc ofset -0.5 V.
I also have a question.
1). From "TI Designs Continuous-Wave Phase-Aligned Multitone Generator: DC-to-6-GHz RF-Sampling DAC Reference Design"
page 6 - "Two DC blocks can be set with amplitudes of 1 and 2."
I correctly understood that DC block is SPI constant value SPIDAC ?
2). Can i generate single tone without JESD204 interface?