In my design I'm using 1K resistors in series on both AIN_nP and AIN_nGND inputs along with a small cap as recommended in the datasheet. To get the maximum possible accuracy AIN_nGND will be grounded remotely at the signal side.
I understand that the working signal on AIN_nGND must be in -0.3V to +0.3V range. I'm a little concerned about somebody accidentally connecting AIN_nGND to significantly higher voltage, let say reversing inputs and getting up to 10V on AIN_nGND. Datasheet shows clamp circuits on both inputs, so there is some protection already and 1K resistor would limit the current to 10mA. Is it a good idea to also add two Schottky diodes connected in parallel in opposite directions on my board between AIN_nGND and the board signal ground for an added protection level?