Dear Sir or Madam,
In one of our devices we use 96 LMP90100.
The LMP90100 is configured for multiple channel continuous conversion. We are facing problems using the LMP90100 near the external climate chamber temperature of -40 °C. Our measures indicate an internal device temperature near the ADC about -35 °C. So we are not operating outside of the specified temperature range.
Our problem is that on some of the ADC (10% of 96 ADCs) we measure disturbances up to 12 uV. We use a ratiometric measurement and therefore we can exclude problems with our reference voltage.
An interesting fact is that those disturbances only appear when we operate the device at a temperature cycle from -40°C up to 85 °C and down to -40 °C. The problem doesn’t always appear on the same ADC. When a new temp cycle is done, it is possible that ADC with problems are good and some good ADC may cause problems. The disturbances appear only at -40°C (climate chamber temperature ). At the other calibration points (5°C, 23°C, 45°C and 85°C) the results are perfect!
We’d like to know if there are any limitations or known issues operating the LMP90100 on such alternating temperatures or what you think in general about our operating mode. If you would like to have schematics or source code for the ADC registers please contact me personally.
Kind regards
Miguel Cabrita