Part Number: DAC37J82
Other Parts Discussed in Thread: DAC5675A
Is there a typo in the datasheet for the frame assembly format for LMF 222 ? There is no mention of Q1[7:0], whereas Q0[15:8] appears twice.
Is the frame format written in red for Lane 1 in the attached photo correct ?
I am migrating from an LVDS based DAC (DAC5675A) design to JESD DAC (DAC37J82) design. The sequence of the complex data sent to the LVDS DAC was I_P -> Q_P -> Q_N -> I_N
I_P <= {~I [15], I [14:0]};
I_N <= {I [15], ~I [14:0]};
Q_P <= {~Q [15], Q [14:0]};
Q_N <= {Q [15], ~Q [14:0]};
Is the below frame assembly format correct for this implementation ?
| Lane 0 | I_P[15:8] | I_P[7:0] | Q_N[15:8] | Q_N[7:0] |
| Lane 1 | Q_P[15:8] | Q_P[7:0] | I_N[15:8] | I_N[7:0] |