This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3424: Analogue Input Insertion Loss

Part Number: ADC3424

Hi guys,

I'm designing a 4 channel amplifier with ADC circuit using the ADC3424 and in the datasheet it recommends an input circuit that it says should be designed to minimise insertion loss. Would it be sensible to change the values of the two resistors connected to VCM (circled in red)? And what is the maximum these should be?