Hello,
We are using the TLA2024 as part of one of our products.
In order to test this product after production, we wish to perform a health check of the TLA2024 that is installed in it. To do so, we were thinking about reading the Configuration Register (RP = 01h) of the TLA2024 and check that it is the expected value. According to the datasheet, this value should be "8583h" after a reset.
However, tests on our side show that this register can take a different value after reset (in this case, we power-cycle the VCC). In particular the value "B5B3h" can sometimes be read in the Configuration Register after a reset of the TLA2024.
Is this to be expected, or should we consider such a component to be faulty? Additionally, if there is a better TL2024 health check process you can suggest I would be interested in knowing about it.
Best regards,
Florian