This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: How to wire the output of myoware and FSR sensors with the input pins of ADS1299 ?

Part Number: ADS1299

I am using two TI ADS1299 and i need to connect the output of the MyoWare and FSR400 sensors with the ADS1299  and i wonder if i need an RC filter like for the EEG signal.Also I didn't understand the where is the bias electrode and the reference electrode while working with the MyoWare and FSR sensors?Can anyone help me?

  • Hello Sarra,

    Thanks for reaching out and welcome to the TI e2e forum!

    I have not worked with Myoware and FSR sensors.

    For the typical EEG data acquisition application, please refer to Figures 72 and 73.