Dear e2e support,
I've got a problem with the DAC8750. We are evaluating the DAC8750-EVM. The Eval.-Board is connected with a STM32L452RE Eval.-Board.
The SPI connection works fine. Initialization, setting the output... everything is possible.
We work in the 4-20mA mode and simple output changes are working,
but if I want to change the output value every 100ms, the DAC crashes after 150-200 cycles and the output is 0.0. mA.
How can I solve this? The SPI connection fine I think. Or is there a overflow?
The SPI init.
The commented out code works fine.
SPI Connection on oszilloscope
Thank you very much!