This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hallo,
Can you tell me how the ADS1675 behaves when the maximum temperature is exceeded?
which parameters change after the maximum temperature is exceeded.
The point is that once the maximum temperature is exceeded, the temperature will drop, but the ADS1675 will continue to operate.
Thanks. Alex
Hello Alex,
Let me see if there is any additional data that we can share.
I will provide an update no later than Monday, Sept 14.
Thanks!
Keith Nicholas
Precision ADC Applications
Hello Alex,
I dug through the original test data for the ADS1675. Unfortunately, there was no data for temperatures above 85C.
Figure 28 in the datasheet does provide some guidance on the change in THD and SNR over temperature.
Regards,
Keith