I've installed the main program and the device package, however the program still isn't detecting the board. I tried to flash the board with the firmware.bin file for the board definition but it erased the current firmware and then failed saying "The USB DFU Drivers are not installed!" I didn't see this driver on the TI website and when I installed the main program it said it was installing all drivers as well, so I'm not sure what's wrong.