Part Number: ADS8681EVM-PDK
Other Parts Discussed in Thread: TMDSLCDK6748, TMS320C6748, ADS8681, BP-DAC11001EVM
I have sensor signal (Acceleration) in analog domain and want to implement a digital filter using DSP kit (selected TMDSLCDK6748) and generate the Analog Output.The required sampling frequency is minimum 50ksps and Input & Output voltage range (-10v to +10v).So my queries are
1.To acquire +10V to -10V range analog signal i selected ADS8681EVM-PDK kit. So is this kit can be configureble with TMDSLCDK6748 and can acquire the data for my requirement?if not can you suggest other module/other possibility?
2.Similarly for output(in Analog) i selected BP-DAC11001EVM, is it ok? if not suggestuons please.
Thank you in advance,Hope i will get the solution at the earliest