This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3482EVM: Example waveform using TSW1400 is not what was expected

Part Number: DAC3482EVM

After some difficulty in getting the registers to load (see previous postings), I finally got everything (DAC3482, CDCE62005 and TSW1400) configured as described in the DAC3482EVM manual (Section 3.4 - DAC348x Example Setup Procedure).  This produced an output that looks somewhat related to the correct waveform.  However, it seems like something saturating or the data capture is introducing some errors.  I tried a number of different registers adjustments to see if I could resolve the problem.  Most of my register changed altered the output spectrum (so I am changing things!), but none were correct.   The spectrum I'm getting when I use the precise register values specified in the EVM manual is the following:

Of course, from the EVM manual, what I'm expecting to see is:

Any suggestions appreciated.