in the data sheet appears the section with the following text "and each channel can be configured as a current or voltage input with software configuration" i have a 4-20 ma sensor , how to configure current input by software .
thanks in advanced
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
in the data sheet appears the section with the following text "and each channel can be configured as a current or voltage input with software configuration" i have a 4-20 ma sensor , how to configure current input by software .
thanks in advanced
Hi Emesto,
The section 9.2.2 in page 55 of ADS8688 datasheet describes a reference design based on ADS8688 precision ADC(TIDU365, the web link in the datasheet for this design TIDA -00164 is directed an incorrect reference design TIDA-01333), this section mentions that this reference design can measure a voltage or current input including 4-20mA and 0-20mA. If we look at the section 5.1.2 and schematic of TIDU365, when measure 4-20mA current input signal, the host controller will control the switches(TLP3123) by TCA6408A to turn on a 200ohm shunt resistor on the input, converting the input current to 0-4V voltage signal to ADS8688 with a full-scale range of 5V. Please refer to below block diagram.
ADS8688 is a precision 8-ch,16-bit ADC and only support unipolar or bipolar single-ended input voltage signal.
Thanks.
Best regards,
Dale