This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM98620: expression on datasheet

Part Number: LM98620

Hi there,

let me ask two questions about the datasheet expression below,

(1) In the Table 50 on page 50,

The Reg0x04 [3:2]bits are for Clock Rage Select. The frequency range mentioned is 10MHz-65MHz, but this device supports the frequency up to 70MHz. Would you tell me the register value for the 65MHz-70MHz.

(2) In the Figure 38 on page 45,

The SDO signal of SPI will be Hi-Z during write operation. But it is changed in the Figure 38 at the D7 data timing. What does it mean?

thank you in advance.

Regards,

  • Hi,

    Let me check your question and feedback to you by Nov 16th.

    regards

    Shinya

  • Hello,

    1) Reg0x04[3:2] = 00 will select 40MHz to 70MHz

    2) SDO will go HiZ  after the A0 clock and does not affect SDI received data .. The data bits  Tih and Tis should be >=5nS

    Regards,

    Costin

  • Hello Costin,

    Thank you for your quick reply.

    1). OK, I'll try it.

    2). You mean that SDO in write mode will go Hi-Z after the first SDI 8bits arrived, because these bits indicate the R/W mode to the AFE.

    So that, dose the SDO keep "Low" or "High" until any command input (SCLK/SDI/SENB changed)? How does it work after any instruction finished?
    According to Figure 39, the SDO seems to be "Hi-Z" in the period except for actually outputting.

    Regards,

  • Hello Costin,

    Thank you for your quick reply.

    1). OK, I'll try it.

    2). You mean that SDO in write mode will go Hi-Z after the first SDI 8bits arrived, because these bits indicate the R/W mode to the AFE.

    So that, dose the SDO keep "Low" or "High" until any command input (SCLK/SDI/SENB changed)? How does it work after any instruction finished?
    According to Figure 39, the SDO seems to be "Hi-Z" in the period except for actually outputting.

    Regards,

  • Hi,

    The SDO is non HiZ mode after a read command, selected device driving D7-D0 on SDO. Rest of the time in read/write mode SDO is HiZ to allow multi device operation.

    Regards,

    Costin

  • Hi,

    Thank you for your kind support.

    I understand and don't mind the unexpected change of SDO in the above Figure 38.
    Your answer makes me clear to use the SDO sharing with another device.

    Regards,

    az