Part Number: ADS5403
We have implemented an FPGA/ ADC design using the 5403. We see an offset occurring on each odd / even sample , the offset is of the magnitude (but not exactly) of 16 to 22 counts. We are able to change the timing of the delays for each output line in the FPGA and we have proven that his works. However, the only difference when we are changing tap values is that the offset moves from even to odd samples - but is still present. We have shown that all lines function and are not 'stuck' in one state or another, so there are no shorts on the board.
Has anyone else come across a similar issue?
Thanks in advance.