Folks,
We've noticed that at power-up, the ADS5407's LVDS outputs are driven to approximately 1 Volt, even though the ADS5407's enable input is driven low. Is there any way that we can turn the LVDS outputs off or at least ensure that the ADS5407's LVDS outputs are always below 0.6 Volts at power-up? We've tried shutting down the LVDS output drivers, but this can only be done after power-up by writing to registers 66 and 67, and even when we did this there was still around 1 Volt observed on the LVDS output signals.
Regards,
- Mike A.