This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7851: Can I use a different VCM than the 2.5V specified in the datasheet

Part Number: ADS7851


Hi, 

I am using ADS7851 and noticed that in the datasheet the maximum input is 2* Vref or AVdd. I then noticed the VCM is spec'd very tight around 2.5V. If I need to make my common mode voltage 3.3V (or some other voltage other than 2.5V) would I be able to with this device as long as I don't exceed the input voltage range limits? I see that the internal reference is set to 2.5V, is this the limiting factor, as with a different VCM then you reduce your full scale range?

Thanks, 

Jose