This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Specialists,
Our customer is considering ADS1217 and has a question.
We would be grateful if you could advise.
---
According to the datasheet P.13 CLOCK GENERATOR, ADS1217 can use oscillator for clock source.
In this case,
How should the XIN and oscillator be connected.
How should XOUT be connected.
Please let me know if there are any other points to note.
Could you please provide an connection example.
ーーー
I appreciate your great help in advance.
Best regards,
Shinichi
Hi Shinichi,
Connecting an external clock source is not complicated. When using an external clock source, such as an oscillator, connect the output of the oscillator to the XIN pin of the ADS1217. The XOUT pin would be left floating as XOUT is only used for crystals or resonators.
The only consideration are the voltage levels and you must match the levels relative to the DVDD supply of the ADS1217.
Best regards,
Bob B
Hi Bob,
Thank you for your reply.
I'm happy to get in touch with you.
I understand how to connect an external oscilator.
I'll share this information with the customer.
I appreceiate your great help and cooperation.
Best regards,
Shinichi
Hi Bob,
The customer has an additional question.
Could you please let me know if you have any information.
Are there any users using ADS1217 with an external oscillator.
I appreciate your great help and cooperation.
Best regards,
Shinichi
Hi Shinichi,
There are advantages of using an external oscillator for several reasons. Generally startup issues over temperature are resolved due to loading on the crystal that may not start oscillation properly. Another reason is due to drift as the external oscillator can be better tuned to stay at a particular frequency with a low jitter output. A third reason may be to synchronize multiple devices to the same clock and timing.
It is difficult to say how may customers have used the external oscillator, but it has been done in the past.
Best regards,
Bob B
Hi Bob,
Thank you for your reply.
External oscillators have several advantages, so I think they are used by various customers.
I appreciate your great help.
Best regards,
Shinichi