Hi,
I want to use ADS62P49EVM to capture sample data with a logic analyzer. To do that I want to avoid SAMTEC connector used on TSW1200 and use instead the J1 and J2 headers available on this evaluation board.
In order to use this two headers the board user's guide says that two CMOS buffers must be installed in place of a bank of 0-ohm resistors.
So, my question is, what i need real to do, to evaluate this board with in that way? There are some kind of option on the buying moment to choose if the buffers are mounted or not? Or I have to buy the "normal" version and then buy separately the two buffers. And if this is the way to do it, I have to solder the buffers to the board, or just plug them on some kind of connector??
Thank you for the support.
Regards,
Diogo Ribeiro