Hi,
I received TSW1200 Source Serial v1p5 from Richard.
The problem is I need to modify the firmware code.
I want to know follwoing questions:
1) are ads5463.ucf, ads 5463_ddrif.v, ads5463_toplevel.v and other verilog codes compatible to ADS4226EVM?
2) is the PROM file generated from the TSW1200 Source Serial v1p5 exactly same with the bit file of TSW1200 in my hand?
3) I ordered a DLC9G programming pod. Is that all to store new FPGA programming bit file?
4) What source code should I modify to change the raw data? For example, I want all data to be deducted 10 from the original value.
5) I need to connect an external DAC through SPI. Are there free pins that I can send some signals after a cycle of ADC finished?
6) I found following line in ads5463.ucf, is that valid for ADS4226EVM?:
TIMESPEC TS_ClkDDRp = PERIOD "ClkDDRp" 2.5 ns HIGH 50%; #ADS528x at 800Msps
7) Is there a programatic way to change the AC-coupling mode into the DC coupling one as we can the same thing in use of an oscilloscope?
Sorry for my too much questions.
Regards,
Euncheon