Hi,
I want to use ADS4226 as ADC to interface with 2.5V FPGA IO's. I am using ADS4226 as CMOS or Parallel. since ADS4226 gives 1.8V digital IO's i put SN74CB3T16210 between ADS4226 and FPGA 2.5V IO's.
I did SI analysis between ADS4226 and SN74CB3T16210 with and with out 22 ohms termination and I do not see a square wave but a sawtooth wave. but ADS4226 LVDS shows a square wave with termination. but i want to use it as CMOS or Parallel only. please suggest how i can make my SI result better.
thanks