We are in the process of evaluating the AFE5807EVM, and are having issues getting either it or the TSW1250EVM to work correctly (not sure which is having the issue).
When I set the AFE5807EVM GUI to output the "Ramp" test pattern, it appears correctly in the Time Domain window of the TS1250 GUI, but then when I input a ~80mVp-p, 5 MHz signal into the ADC, it is "flattening" the peaks/valleys of the signal, basically converting it into a square wave that goes from the lowest (0) to highest (4096) value in the window.
Is there some setting I'm missing somewhere?
I've attached a word doc with screenshots of each tab in the AFE5807EVM GUI as well as the TSW1250 GUI.