Dear All
I' using an ADS1014 (12bit 3.3ksps) in a nosily application and I need to design an analog low pass antialias filter for its inputs. Because I don't want to add offset and non linearity to the system I would like to design the input filer with analog components only. Because the converter is put in a feedback control loop should be better if the phase of the low pass filter would be linear enough with the frequency. A need to use the max available bandwidth (3.3k/2 = 1.5ksps) and an attenuation of 6dB/bit*12 bit = 72dB at the Sigma-delta unknown sampling frequency
1) Does TI has a tools to calculate this filter ?
2) Dows Ti suggest a tools to design such filter ?
2) What is the sigma delta modulator sampling frequency of the ADS1014
Thanks
Paolo