Hello I am using the ADS1296 with bipolar supplies +/-2.5V. So AVDD = +2.5V, AVSS = -2.5V. There are 2 possible settings for the ADS1296 voltage reference (VREF) in CONFIG register 3 bit 5.
a) If bit 5 is 0 = VREFP is set to 2.4V
b) If bit 5 is 1 = VREFP is set to 4V (use only with a 5V analog supply)
Questions:
Q1) Which setting should I be using to maximize the input dynamic range of the AFE?
Q2) When the datasheet says 5-V supply, do they mean +/-2.5 or 5V?