Part Number: ADS1299
Greetings
Our team has a 8 channel prototype EEG working well using the ADS1299 Very nice chip and easy to implement (once one learns the registers!).
My question regards the single shot, RDATA mode. We will add another chip to get to 16 channels (eventually 32). For several reasons we would like to use the single shot mode rather than daisy chain.
Section 9.5.3.9 RDATA: Read data of October 2016 data sheet (page 41) implies that the START PIN (number 38) must be made high to start the data conversion and held high through the complete reading of the data. Is that correct?
Also - there is an option to use the START command on SPI. I am unsure regarding using the START command. Can it be sent to two chips at one time? I have never done that with SPI and am not sure it is allowed. Also is the STOP command required on completion of the data retrieval?
I will bit bang through this if necessary but comments are appreciated!
Thank you
Tom Schmitt
Atlanta, Georgia
USA