This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TP27 is 24VDC, AIN0 measured at 2.197V +/-4.096 FSR (2mV per LSB), ADC is set read AIN0 re GND. Should read 1090base10 (0x4420), reads 66base10 (0x1022), I2C config command is i2cset -y 0 0x49 0x01 0xC383 w, I2C read command is i2cget -y 0 0x49 0x00 w.
Where did I go wrong?