Hi,
I’ve analyzed calibration_AFE4404.c to figure out the main concepts. But to apply this code to my HW (SFH7072), the following constant values should be clarified.
1. ADC_CODE_AMB_DAC_MIN, ADC_CODE_AMB_DAC_STEP are defined initially with some values.
Can these values be used for any LED-PD module ? How these values were obtained ? (by calling OFFSET_DAC_Code_Est ?)
Theses two values are commented out in ‘OFFSET_DAC_Code_Est(), it means the initially defined values are used instead of calling OFFSET_DAC_Code_Est().
2. Regarding Ipleth_array[5], this array have predefined values.
How these values were obtained ? (by measuring or by calculating something ?)
Are theses values valid for any LED-PD module ?
3. Regarding Meas_DC_1K_1code_10CTR and Meas_DC_1K_500nAPleth,
What are the meanings of them ?
How the values were obtained ? (by measuring or by calculating ?)
Are the values valid for any LED-PD module ?
Thanks in advance.
Konan