Hi,
I am interested in designing a daisy chain of ADS8688's to measure the voltages 48 batteries, which are wired in 8 parallel columns of 6 series batteries each, to power some motors. The batteries are roughly 1.5 V, so each column will be 9 V. The batteries voltages will drop as the experiment runs (roughly 4 minutes). I like the ADS8688 because it can measure up to +/- 10.24 V and it can measure differential inputs. My research team and I have also experienced battery polarity reversal on some batteries, so being able to measure negative inputs is extremely valuable, which the ADS8688 can also do. Also, the sampling rate is unimportant as we are just looking for anything at this point. I just have some basic questions that I was hoping I could get answered before I go ahead and begin building this device:
1. I mentioned that my measurements may experience negative voltages. Will the MSP432 be able to measure a possible negative voltage of say -1.5 V? I am not interested in inverting that result, so if the MSP432 would not work, do you have something else in mind that could help me? My internet research is not proving to be helpful.
2. Is it possible to connect 12 ADS8688's to an MSP432 and write a code to extract the data we need? My knowledge of the MSP432 is limited, but good enough that I think I could figure out the code; I just want to know that it will work before I try. If there aren't enough pins, would you suggest using a multiplexer, and, if so, do you have one in mind?
3. I know that I can use to MSP423 to provide 5 V to the ADS8688's. Do you think I would run into problems with drawing to much current from the MSP432, or is that something I do not need to worry about?
4. I am worried about the accuracy of my results. In the measurements, we never look past the thousandths decimal place. Do you think with 16-bit resolution at 5 V, we should be able to safely measure at least 3 decimal points?
Thank you in advance for any help you can give and me please let me know if you have any questions for me or need something explained in more detail.
-Spencer