Other Parts Discussed in Thread: TS3A5017, DAC81416
Hi,
Can I use single DAC8718 and use SP4T switch (similar to TS3A5017) at each analog output, so I can have 32 outputs from single DAC8718.
If possible please suggest an analog switch.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dinesh,
This can work, but note that the DAC will only drive one of the outputs at time, so if you want a steady state voltage on each of the outputs you will need a sample-and-hold type circuit.
You could also consider (two) devices like the DAC81416, which is a high-voltage, 16-channel, 16-bit DAC.
Thanks,
Paul