This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TLC7528: 4-quadrant operation

Intellectual 3000 points

Replies: 3

Views: 238

Part Number: TLC7528

Hi team,

Customers want to use TLC7528 chip to generate modulation wave: the reference voltage is ±2V, duty cycle 50% square wave, square wave frequency is a fixed frequency between 2-12KHZ; the output is bipolar wave with variable peak value.

Questions:

Can TLC7528's 4-quadrant operation be powered by a single power supply?

Does TI have a 4-quadrant operation ADC chip that can be powered by a single power supply?

The output waveform is similar to the following waveform:

Best Regards,
Amy

Best Regards,
Amy Luo

  • Hi Amy,

    Thank you for your query. I am looking into your issue. I will get back by tomorrow.

    Regards,

    Uttam Sahu

    applications Engineer, Precision DAC

  • In reply to Uttam Sahu:

    Hi Uttam,

    Is there any update?

    Best Regards,
    Amy

    Best Regards,
    Amy Luo

  • In reply to Amy Luo:

    Hi Amy,

    Apologies for the delay in response. Last week was very crazy. The DAC operates with single-supply. The bipolar or 4-quadrant operation can be achieved with the circuit as shown in your post wherein the output amplifiers are bipolar. So, if you mean whether we can achieve bipolar operation using single-supply amplifiers, the answer is no.

    Regarding the ADC, you need to post a query in the ADC forum.

    I hope that answers your question. Let me know if I have misinterpreted your question.

    Regards,

    Uttam Sahu

    Applications Engineer, Precision DAC

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.