Hi, I'm triying to use dac7760 and alarm pin is always in low state so dac not work. when i try to read status register there is no data come from dac. Is that mean dac was damaged or is there any other thing that alarm pin need to goes high.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I'm triying to use dac7760 and alarm pin is always in low state so dac not work. when i try to read status register there is no data come from dac. Is that mean dac was damaged or is there any other thing that alarm pin need to goes high.
Hi Furkan,
This could mean many things. Most likely the device is not fully powered on or is still in the POR state. You should verify that all the supply pins are valid. You should also confirm that the SPI command is correctly formatted.
Thanks,
Paul
Hi Paul,
Thank you for your answer. DAC supply with 24 V and 5V and there is no problem with supply. I looked SPI signals with logic analyzer and there is also no problem with spi data. For the initial settings I tried these settings. If dac is in POR state. How to fix that problem or do you have any other suggesitons.
// 0x56 Write reset register WriteSingle_DAC7760(0x56, 0x0001); // 0x55 Write control register WriteSingle_DAC7760(0x55, 0xB001); //0x57 configuration register WriteSingle_DAC7760(0x57,0x0B00);
Hi Paul;
Thank you. I take new DAC7760 now alarm pin give 5v But still DAC not work properly . Output gives 0.5 V always. I supply 24V for AVDD from power supply. Also 5V for DVDD from stm32. Is that enough for DAC? Now the main problem is DAC show any response for SPI datas. SPI datas are correct i checked with logic analyzer. If power is enough and DAC is in POR state how do i know that and how to fix that?
Hi Furkan,
Can you share the SPI transaction? Can you also monitor the LATCH pin as well? It will be useful to have another engineer look at it. What is the voltage on the REFIN pin?
Assuming everything is connected correctly, the device should be responding. If it is not responding, then we must assume:
1. It is not powered on or there is an assembly issue
2. the SPI is not formatted correctly
3. the device is damaged
Thanks,
Paul
Thank you Paul I solve my problem. The problem was spi connections. Before changed the DAC i changed spi configurations and After changed chip i was reconfig the spi and it worked. Sorry for my english and late response.