Dear Forum,
I am using a DDC112 to measure the current flowing through a fixed resistor. The source voltage (0.5V) and resistor (201k Ohm) are very stable and precise.
I have tested many resistors (up to 1GOhm ) and have always the same strange issue with the measured values.
The values from the same integrator are almost identical to each other, but the difference between the integrators is about 5% (this happens with internal and external capacitors alike). This is the same with channel 1 and 2. In test mode, I observe the mentioned 0.2pC difference, and all seems fine.
What can cause this issue?
Best regards
Christof