Hi everyone,
I'm using the ADS1292R now. I noticed that the IN1 should be applied as the respiration signal input, and the IN2 still can detect the ECG.
I want to use the RLD when acquiring the ECG. In the datasheet, I found an example that the RLD signal could generated from channel 1 and routed to the N-side of channel 2.
So I want to make sure if the IN1 could still be used as the RLD signal source while acquiring ECG, even though the IN1 is applied to the respiration?
Thanks a lot,
Yuhang.