Hello Team
I am working on a system for pairing and selection of optocouplers. I work with 8 optocouplers per test cycle and I use 2 ADS1115's single ended in continuos mode at 860sps. After a settling period of 15 secs all 8 channels are measured, waiting 3ms after each input switch. This pattern is repeated 10 times and the results are averaged. 860sps is chosen because all 80 measurements must be done within less than ½ sec. This setup does function ok, but some noise is introduced from the opamps in the signal conditioning circuitry, so I intend to add a unity gain buffer with RC lowpass filter to each channel.
As a SPICE model of the ADS1115 cannot be found I would like to make a simulation model of the ADC input to help me choose the best opamp/filter combination, and for this job I need some information.
As I understand from the datasheet the sampling frequency is 250KHz giving a total sample time of 4 microseconds. In this period we will have an aquisition period, a hold or conversion period and finally a discharge period. I suppose this pattern is repeated many times during the 1.1ms needed for the 860sps and then averaged ?
What I would like to know is:
1. the aquisition time 2. the conversion time 3. the discharge time 4. the timing between the three. and 5. the values of the capacitors in the input.
Thank you very much in advance
Ole Palmhoej