Hello,
I'm using the ADS1256 in my design and I have used crystal to generate ADC's clock.
I followed recommendations from data sheet and evaluation module for clock generation. I have used 7.68 MHz crystal with same properties and parallel capacitors of 18 pF as like as crystal used in EVM. My problem is in fact that oscillator will not start every time when I turn on board power supply. One of ten times it fails.
Start up time of 3.3V power supply for digital side and +5V of analogue side is less than 10 ms and both power supplies turn on and off correctly (no spikes, voltage drops,..).
I checked load capacitance for my crystal and crystal used in EVM. Both have 18pF load capacitance.
I assuming that parallel capacitors of 18 pF used in EVM (also used in my design) are not enough to start up oscilator to oscillate.
According to definition: CL=(C1*C2)/(C1+C2) +Cstray. For C1=C2=18pF CL equals 9pF+Cstray where Cstray can be between 3 to 5 pF. So, the maximum value for CL will be 14 pF in best case. Manufacturers of crystals recommend CL to be as close to possible to Cl of crystal.
Can you comment this problem?
Thanks in advace.
Josko Marasovic