Part Number: ADS1293EVM
Other Parts Discussed in Thread: ADS1293, ALLIGATOR
Hello. I have been using the TI ADS1293EVM board to acquire signals from a USB waveform generator (Analog Discovery module from Digilent [https://reference.digilentinc.com/reference/instrumentation/analog-discovery/start?redirect=1]). I performed a voltage (from 0.1 mV - 50 mV pk-pk sine wave with 0V offset) and frequency sweep (from 10 - 200 Hz) to characterise the ADS1293EVM.
I find that the amplification factor/gain of the ADS1293EVM varies as a function of frequency and is not equal to the value of 3.5x as mentioned on page 15 of the ADS1293 datasheet. Is this normal/expected or am I doing something wrong? I measured the output from the waveform generator using a scope and the voltages were what I expected them to be.
I have attached a couple of figures as well as a CSV file of the data I measured. The values of mean and pk-pk output voltage measured are obtained from the ADS1293 software's "Measurement" tab.
Thanks and regards,
Ganesh Raam