Other Parts Discussed in Thread: DAC38J82, DAC38J84
Hi,
I would like to know if I can configure the DAC37J82 for my use case:
JESD Lanes = 4
DAC Sampling frequency = 819.2MHz
For channel 0 and channel 1:
Input IQ signal DataRate = 409.6MHz (interpolation=2)
Input IQ signal actual Bandwidth = 96MHz
Output RF center frequency [70MHz - 160MHz] (ie actual signal would be at maximum between 70-96/2=22MHz and 160+96/2=208MHz).
1)Is this configuration achievable with DAC37J82 ?
2)Is there 2 independant NCO like the documentation says ?
"The DAC37J82/DAC38J82 has two full complex mixer (FMIX) blocks with independent Numerically Controlled Oscillators(NCO)".
Or just one and I won't be able to have different output center frequencies for channel 0 and channel 1 ?
Thanks