Hello
I would like to use ADS122C04 in one of my applications for input voltages +-2.048V or less. I am power suppling with +-2.5V on analog part and 3.3V on digital part. Will I have the range from -2.048 to +2.048V with using internal reference voltage which is 2.048V? This is the case where I use AIN0, AIN1 and AIN2 as voltage input AINp and AIN3 connected to 0V (GND) as AINn. In this combination 3 channels out of four. What happens with the input range if I use AIN0..AIN3 as AINp and internally connect all AINn to AVSS which would be in my case -2.5V? In this case I have all four channel available.
Best regards
Simon Mali