Other Parts Discussed in Thread: ADS1298
Hi Team,
Customer is using ADS1292 / QFN32 chip. AVDD-AVSS | DVDD-DVSS are powered by + 3.3V, internal clock is selected. CONFIG2. The PDB_REFBUF bit has been set to 1, and the reference voltage is selected to be 2.42V. Digital SPI communication sequence is normal, ADS1292 can normally generate data ready interrupt. The channel data read are: Channel 1: 0X7FFFFF Channel 2: 0X800000 (channels 1-2 are all floating).
Question: Use a multimeter to measure the voltage between VREFP and VREFN (GND) to -0.075V.
Thanks,
Annie