Other Parts Discussed in Thread: ADS1261
Hello,
Assume that VREFP is connected to an ideal +2.5V reference and VREFN is connected to AGND.
Assume that the range of the input signal is from 0V to 5.05V, which is also the voltage at AVDD. (This is arbitrary, but for this hypothetical situation we can assume that it won't reach the level at which the ESD diodes conduct.)
The signal range is thus larger than the reference voltage * 2.
Assume that SELFCAL has populated the FSC registers.
Is it possible to scale this FSC calibration data so that the 5.05V signal (that is outside of the reference voltage * 2 but within AVDD-to-AGND) can be accurately read?
Best regards
Niclas