This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE58JD18: Supply bypass caps

Part Number: AFE58JD18

In the AFE58JD18 datasheet, it says "Bypass all supply pins with 0.1-μF ceramic chip capacitors (size 0603 or smaller)." I read that as, for every supply pin, one should add a bypass capacitor. However, in the EVM design, this doesn't seem to be the case. For example, the 5VA rail has 7 pins on the device, but only 4 capacitors on the EVM Decoupling schematic. 

Given the EVM is a reference design, is it OK follow this example? 

On a similar note, I see there isn't a via for every power or ground pin of the device, but instead power and ground pins are grouped together with traces or polygon pours sharing a subset of vias. Again, I want to be sure it's ok to follow this example.