Hi,
We use DAC device with 4 lanes 0-3 , DAC A/B (C/D are not used).
After configuring the device we poll register 0x6c to see if DAC function as expected(read is after write to clear).
Value of register 0x6c varies after every configuration : sometimes value is 0x05 and sometimes 0x07.
Bit 1 is defined by Datasheet as reserved.
By the way regs 0x64-0x67 are all zeros.
Does it point on a hidden problem or an issue that needs attention ?
If YES , where should be look for it ?
Thanks
Tamir